var oldLink = null;


// This function gets called when the end-user clicks on some date.
function selected(cal, date)
	{
	lstrInputFunction = cal.sel.id + "_change";
	cal.sel.value = date; // just update the date in the input field.
	if (cal.dateClicked)
		{
		cal.callCloseHandler();
		eval("if (typeof(" + lstrInputFunction + ")!='undefined'){" + lstrInputFunction + "()}");
		}
	}

// And this gets called when the end-user clicks on the _selected_ date,
// or clicks on the "Close" button.  It just hides the calendar without
// destroying it.
function closeHandler(cal) {
  cal.hide();                        // hide the calendar
//  cal.destroy();
  _dynarch_popupCalendar = null;
}

// This function shows the calendar under the element having the given id.
// It takes care of catching "mousedown" signals on document and hiding the
// calendar if the click was outside.
function showCalendar(id2, id, format, showsTime, showsOtherMonths, disabledDateHandler) {
  var el = document.getElementById(id);
  if (_dynarch_popupCalendar != null) {
    // we already have some calendar created
    _dynarch_popupCalendar.hide();                 // so we hide it first.
  } else {
    // first-time call, create the calendar.
    var cal = new Calendar(1, null, selected, closeHandler);
    // uncomment the following line to hide the week numbers
    // cal.weekNumbers = false;
    if (typeof showsTime == "string" || showsTime == true) {
      cal.showsTime = true;
      cal.time24 = (showsTime == "12" ? false : true);
    }
    if (showsOtherMonths) {
      cal.showsOtherMonths = true;
    }
    _dynarch_popupCalendar = cal;                  // remember it in the global var
    cal.setRange(1900, 2070);        // min/max year allowed.

	// custom function to manage disabled dates
	// see \msFormBuilderElements\msDaterange.class.php
	// for an example of it's usage
	if(disabledDateHandler != null)
	{
	  cal.setDateStatusHandler(eval(disabledDateHandler));
	}

    cal.create();
  }
  _dynarch_popupCalendar.setDateFormat(format);    // set the specified date format
  _dynarch_popupCalendar.parseDate(el.value);      // try to parse the text in field
  _dynarch_popupCalendar.sel = el;                 // inform it what input field we use

  // the reference element that we pass to showAtElement is the button that
  // triggers the calendar.  In this example we align the calendar bottom-right
  // to the button.
  _dynarch_popupCalendar.showAtElement(id2, "BR");        // show the calendar

  return false;
}

var MINUTE = 60 * 1000;
var HOUR = 60 * MINUTE;
var DAY = 24 * HOUR;
var WEEK = 7 * DAY;

// If this handler returns true then the "date" given as
// parameter will be disabled.  In this example we enable
// only days within a range of 10 days from the current
// date.
// You can use the functions date.getFullYear() -- returns the year
// as 4 digit number, date.getMonth() -- returns the month as 0..11,
// and date.getDate() -- returns the date of the month as 1..31, to
// make heavy calculations here.  However, beware that this function
// should be very fast, as it is called for each day in a month when
// the calendar is (re)constructed.
function isDisabled(date) {
  var today = new Date();
  return (Math.abs(date.getTime() - today.getTime()) / DAY) > 10;
}