SEARCH    
Avnet® Technology Solutions
Avnet Technology Solutions. Distributor of enterprise computing products, software and services

Contact Finder

Avnet contacts found : ?

Storage Hierarchy


The range of memory and storage within and attached to a computer system is known as the Storage Hierarchy and to help understand this further can be categorised into 4 segments. As memory and storage devices move down the hierarchy they reduce in performance and cost/MB or GB but tend to rise in capacity through to the last category which includes removable media which in effect has no restriction on capacity a device can store.

Storage Hierarchy

  • Primary Storage is the top level and is made up of CPU registers, CPU cache and memory which are the only components that are directly accessible to the systems CPU. The CPU can continuously read data stored in these areas and execute all instructions as required quickly in a uniform manner. Secondary Storage differs from primary storage in that it is not directly accessible by the CPU. A system uses input/output (I/O) channels to connect to the secondary storage which control the data flow through a system when required and on request
  • Secondary storage is non-volatile so does not lose data when it is powered down so consequently modern computer systems tend to have a more secondary storage than primary storage. All secondary storage today consist of hard disk drives (HDD), usually set up in a RAID configuration, however older installations also included removable media such us magneto optical or MO
  • Tertiary Storage is mainly used as backup and archival of data and although based on the slowest devices can be classed as the most important in terms of data protection against a variety of disasters that can affect an IT infrastructure. Most devices in this segment are automated via robotics and software to reduce management costs and risk of human error and consist primarily of disk & tape based back up devices
  • Offline Storage is the final category and is where removable types of storage media sit such as tape cartridges and optical disc such as CD and DVD. Offline storage is can be used to transfer data between systems but also allow for data to be secured offsite to ensure companies always have a copy of valuable data in the event of a disaster.

For more information:

Ask the experts

Open Storage

Storage & SAN, Data Protection, Network Storage Solutions, Storage Networking

+ 44 (0) 1344 662 298

open-storage-uk@avnet.com


RAID Controllers

+44 (0)1344 355 800

computer-components-uk@avnet.com


Hitachi Data Systems

Avnet Technology Solutions

+44 (0)1344 355 920

hds@avnet.com


HP

Avnet Technology Solutions

+44 (0)1706 898 398

hp-uk@avnet.com


IBM

Avnet Technology Solutions

+44 (0)1706 222 180

+44 (0)1344 662 230

ibm-storage-uk@avnet.com


NetApp

Avnet Technology Solutions

+44 (0)1344 355 920

NetApp-open-storage-uk@avnet.com


Oracle

Avnet Technology Solutions

+44 (0)1925 856 900

oracle-hardware-uk@avnet.com

 

Symantec

Avnet Technology Solutions

+44 (0)1706 898 398

symantec-uk@avnet.com

LinkedIn banner
Events

What else would you like to see on this page?

Follow us on LinkedIn RSS Follow Avnet TS UK on Twitter YouTube
       

Bookmark and Share