SEARCH    
Avnet® Technology Solutions
Avnet Technology Solutions. Distributor of enterprise computing products, software and services

Contact Finder

Avnet contacts found : ?

Internet Small Computer System Interface (iSCSI)

iSCSI is Internet SCSI (Small Computer System Interface), an Internet Protocol (IP) based storage networking standard for linking data storage systems, developed by the Internet Engineering Task Force (IETF). By carrying SCSI commands over IP networks, iSCSI is used to facilitate data transfers over intranets and to manage storage over long distances. The iSCSI protocol is a key technology that has help to bring about rapid development of the storage area network (SAN) market, by increasing the capabilities and performance of storage data transmission. Because of the ubiquity of IP networks, iSCSI can be used to transmit data over local area networks (LANs), wide area networks (WANs), or the Internet and can enable location independent data storage and retrieval.

How iSCSI Works

When an end user or application sends a request, the operating system generates the appropriate SCSI commands and data request, which then go through encapsulation and, if necessary, encryption procedures. A packet header is added before the resulting IP packets are transmitted over an Ethernet connection. When a packet is received, it is decrypted (if it was encrypted before transmission), and disassembled, separating the SCSI commands and request. The SCSI commands are sent on to the SCSI controller, and from there to the SCSI storage device. Because iSCSI is bi-directional, the protocol can also be used to return data in response to the original request.

The iSCSI storage system is usually referred to as a target and is accessed by other systems across the network via iSCSI initiators; these can be either software initiators embedded within the host operating system or hardware initiators in the form of host bus adapters (HBA’s). The benefit of using hardware initiators is their ability of some HBA’s to offload the TCP/IP activity on to the card thus reducing the overhead on the host CPU. These HBA’s can also be referred to as TCP Offload Engines or “TOE cards”.

Benefits of iSCSI

iSCSI deployments are typically within tier 2 and tier 3 data centres in large organisations, in the core of data centres for small/medium enterprises and also in remote offices. iSCSI has grown quickly  and is usually chosen for environments that Fibre Channel has had difficulty penetrating due to cost, complexity, functionality or support issues.

The application sweet spot has been storage consolidation and virtualisation for business critical Windows environments. Its popularity has not only been driven by the fact you can deploy robust affordable SAN solutions on x86 server platforms, but also because even entry level iSCSI disk arrays usually include sophisticated data management capabilities such as point in time copy, remote copy, thin provisioning and asynchronous mirroring. It is these features that allow organisations to significantly improve storage provisioning, back up and disaster recovery whilst reducing infrastructure and management costs. Besides product features, other benefits include ease of management, unlike Fibre Channel, which needs dedicated support, iSCSI being IP based means current server and applications administrators usually have no problems configuring and maintaining and iSCSI based SAN.

iSCSI has a bright future ahead of it and it will continue to grow and take share from the entry level Fibre Channel market. Current providing acceptable performance on 1GbE, iSCSI will really show its true performance benefits once 10GbE is adopted as standard within data centre and server environments that utilise multi core CPU’s to deliver bandwidth hungry applications such as virtualisation and video streaming.


 Next steps:

Ask the experts

EMC and CommVault 

Avnet Technology Solutions

+44 (0) 1344 662 298

open-storage-uk@avnet.com

Open Storage

Avnet Technology Solutions

+44 (0)1344 662 298

open-storage-uk@avnet.com

Storage Networking

Avnet Technology Solutions

+44 (0) 1344 662 298

storage-networking-uk@avnet.com

Storage Solutions

Avnet Technology Solutions

+44 (0)1344 355 800

computer-components-uk@avnet.com

Syncsort 

Avnet Technology Solutions

+44 (0)1344 355 920

netappuk@avnet.com

http://www.twitter.com/Avnet_TS_UK
Right Bottom Fact sheet

Help us make sure this website is right for you.
If you would like a response to your feedback please submit your email address



Follow us on LinkedIn RSS Follow Avnet TS UK on Twitter YouTube
       

Bookmark and Share