- Home
- Suppliers
- HP
- Our Approach
- Value Propositions
- Mission Critical Computing
Next Generation Mission Critical Computing
Our Value Propositions connect you to the resources that make the deal happen and provide a solid structure for your sales effort.
- HP9000 Migration to Integrity – With HP 9000 going end-of-life Dec 2008, customers have a five-year window to migrate to HP Integrity and reduce server TCO at the same time. HP has made this simple via a rich tool set and over 14,000 applications already migrated.
- Sun Competitive Attack – Customers running SUN for business-critical applications and processes are suffering from the current uncertainty about the future direction of that business, preventing them from making solid decisions about future core computing. HP Integrity offers the certainty that’s missing alongside market leading availability and scalability.
- HP-UX – Whilst the HP 9000 system has gone end-of-life, HP remains committed to HP-UX development so the skills and expertise customers have in HP-UX have an ongoing value, and should be valued and nurtured as part of a migration to HP Integrity.
- Integrity Blades – Business-critical computing meets the efficiency of blades. HP Integrity blades support mission-critical workloads through the use of a range of operating systems that have traditionally supported enterprise applications and databases but also now support new workloads related to Web-enabled computing and collaborative software.
- Business Critical Servers - HP’s next generation, business critical server portfolio delivers the industry’s first mission-critical Converged Infrastructure in one platform – simplifying, unifying and automating IT, from x86 to Superdome 2.
- HP NGIS - Migrating to an HP mission critical converged infrastructure platform, based on HP Integrity / Superdome 2 servers running HP-UX, will reduce the total cost of ownership and deliver better ROI and business agility.
Download our HP Value Propositions summary +
To see the full Value Proposition for a specific area please contact Bonnie Littlewood and add the name of the Value proposition to the Subject line.
For More Information: