HP 9000 Migration to HP Integrity
HP 9000 servers are being discontinued, with a final order date of December 31st 2008.
With this in mind, you need to be talking to your customers about alternative solutions and encouraging them to migrate to HP Integrity. The sales message is both simple and engaging: migrating from HP 9000 to HP Integrity will reduce costs and increase performance.
- Significantly lower TCO
- A fast return on investment
- Substantial performance improvements
- Future proof solution
- Reduce service costs
- Reduce management time
- Reduce floor space requirements
- Reduce energy use & cooling costs.
Calculate the cost of migrating from HP 9000 to HP Integrity
HP Integrity servers = twice the performance of comparable HP 9000 systems
HP Integrity servers = reduction in the number of CPUs / servers required
For example:
8x HP 9000 servers = 4 x HP Integrity servers = 2:1 server reduction
4 x HP Integrity servers + virtualisation = 2 x HP Integrity servers = 4:1 server reduction
If your customers are running an HP-UX environment, calculating the cost of migrating from HP 9000 to HP Integrity is straightforward. Independent research has been undertaken which provides a detailed analysis of the potential benefits of consolidating multiple HP 9000 servers to fewer HP Integrity servers, highlighting the following key results:
- Using HP Integrity servers to consolidate multiple HP 9000 servers running HP-UX pays for itself within a short period of time.
- The vast majority of companies viewed Integrity servers to be just as good or better than HP 9000 servers.
- HP-UX on Integrity is just as easy to manage and reliable as HP-UX on HP 9000.
In summary, any company that has more than a couple of HP 9000 servers installed should seriously consider consolidating these servers into HP Integrity.
For more information, please contact your Avnet Account Manager.
For More Information: