SEARCH    
Avnet® Technology Solutions
HP_ROI_banner_995x160

Contact Finder

Avnet contacts found : ?

Business Drivers

Ageing x86 infrastructures cost more to run and support than many organisations realise – with server sprawl, rising power and cooling costs and increasing management overheads. According to IDC, the purchase price of a server only accounts for 25% of the overall cost of running the system over 3 years. The other 75% is related to keeping it running – managing, powering and keeping it cool. As much as 80% of current x86 servers have reached a mature lifecycle and are ready for refresh. HP is uniquely positioned to deliver leading ROI with solutions optimised to work together and adapt to future technology and business change.

Opportunity Spotting

Customers with an ageing x86 server environment (more than 2 years old):

Their current x86 infrastructure is costing more than they probably realise and investing in the latest HP G7 server technology could help them to reign in server sprawl, rising power and cooling costs and increasing management overheads:

  •  ROI in as little as 30 days against G4
  •  ROI in 8 months against G5.

Customers where power and cooling costs have become a major issue:

The energy efficiencies of HP G7 delivers:

  • Up to 2.5 times more power efficiency than previous generation servers
  • Proactively managed power consumption, with Thermal Logic technology
  • Dynamic power capping – tripling the power capacity of an existing data centre
  • 96% reduction in power and cooling costs.

Customers looking to improve infrastructure manageability through virtualisation:

With a server consolidation ratio of 91:1 or better and a 200% boost on server availability, HP G7 enables your customers to:

  • Achieve more virtual machines per rack
  • Reduce operating expenses with lifecycle management via HP Insight Control
  • Simplify setup and operations with HP Onboard Administrator
  • Decrease virtualisation complexity using HP Insight Server Migration and HP Insight Dynamics VSE.

For More Information:

Ask the expert

Hewlett Packard

Avnet Technology Solutions

+44 (0) 1706 898 398

hp-uk@avnet.com

HPOptionKit_324x202
Financial strength